Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
Hi!
I am working with the latest version of CCS (v8.2). I am trying to build a project that has been working before, but after checking out a different commit from git for a minute and then switching back to the original one I get many many errors and the compilation fails. I've already tried to clean, rebuild, make a new workspace, as well as completely uninstalling CCS and re-installing it, non of those seems to be working, please help!
The errors are too many and repetitive so I am only mentioning a few of them here:
- error #19035-D: unclosed string or character constant
- error #10021-D: expecting filename, option, MEMORY, or SECTIONS instead of "5"
- error #10008-D: cannot find file "["
And the build process ends with the below message in the console:
error #10010: errors encountered during linking; "controller_master.out" not built
>> Compilation failure
makefile:197: recipe for target 'controller_master.out' failed
gmake[1]: *** [controller_master.out] Error 1
makefile:193: recipe for target 'all' failed
gmake: *** [all] Error 2
**** Build Finished ****
I