Part Number: TMS570LC4357
Hello,
We are using the TMS570LC4357, we would like more information about the IOMM module.
In Table 6-3 and Figure 6-8 of Reference manual (spnu563a), ESM1 register can sample nERROR or nERROR1 via PINMMRx.
Nevertheless, in thefollowing sentence is confusing for us:
"By default, the ESM1 Error Pin Status Register (ESMEPSR) samples the nERROR pin input. The default is achieved with PINMMR174[16] = 1. By setting PINMMR174[16] = 0, the ESM1 Error Pin Status register
will sample from the nERROR1 pin instead"
> In Table 4-20 of datasheet, what the differences between nERROR (from ESM error) on pin B14 and nERRO (from ESM error 1) on pin J2 ?
> The reference manual mention the nERRO pin and the nERROR1 pin but this is not the case of datsheet where nERROR is on J2 and B14. Could you clarify that please ?
> Moreover, Why ESM1 sample nERROR pin input altough this is an output and not an input as mentionned in the refrence manual ?
Best regards,
Christopher