This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/TM4C1294NCPDT: NDK - retrieving the default gateway when using DHCP

Part Number: TM4C1294NCPDT


Tool/software: TI-RTOS

I am having difficulties retrieving the the default gateway when using DHCP with the TI-RTOS NDK (TI-RTOS version 2.16.01.14, NDK version 2.25.00.09).

In my hook function that gets called when new IP address info is received via DHCP, I have the following code, which is intended to retrieve the default gateway address:

int Result;

    int NumberOfInstances = CfgGetEntryCnt(0, CFGTAG_IPNET, 1); // success

    if (NumberOfInstances >= 1) {

        CI_IPNET IpConfig;

        bzero(&IpConfig, sizeof(CI_IPNET));

        Result = CfgGetImmediate(
            0, CFGTAG_IPNET, 1, NumberOfInstances,
            sizeof(CI_IPNET), (UINT8*)&IpConfig);  // success
        ...
    }

NumberOfInstances = CfgGetEntryCnt(0, CFGTAG_ROUTE, 1); // fails

if (NumberOfInstances >= 1) {

CI_ROUTE RouteConfig;

bzero(&RouteConfig, sizeof(CI_ROUTE));

Result = CfgGetImmediate(
    0, CFGTAG_ROUTE, 1, NumberOfInstances,
    sizeof(CI_ROUTE), (UINT8*)&RouteConfig);

if (Result) {

    ...
}

}

NumberOfInstances is always zero after calling CfgGetEntryCnt for tag CFGTAG_ROUTE, implying there is no route information in the configuration.

In looking through other forum posts, I see this post below, which suggests using functions Rt* in routeif.h, with function DumpRouteTable in NDK file conroute.c providing an example of how to use those functions. This function and code seems complicated though.

e2e.ti.com/.../1900996

What is the proper way to get the default gateway IP address when using DHCP. Is my code above right, or do I have to do something like what is found in function DumpRouteTable in NDK file conroute.c?

Thanks in advance