Other Parts Discussed in Thread: ADCPRO, ADS1220, ADS1220EVM
Hello, we are using the ADS 1220 EVM board and we noticed that when we use the turbo mode in 2000 SPS the frequency shown in the ADCPRO soft is doubled with respect to the real one.
For example, the frequency of the input signal is 100 Hz and in MULTISCOPE and MULTIFFT 200 Hz is observed (that is, the value of the input frequency is doubled). If you sample at 1200 SPS, 120 Hz is observed
When the sampling rate is less than or equal to 1000 SPS, the presentation is correct, ie 100 Hz.
regards