This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: TMS570LS1224: Program Flash

Part Number: TMS570LS1224

The datesheet 6.10.5 twec Write/erase cycles with 15 year Data Retention -40°C to 125°C 1000 cycles requirement 。

it means one chip, Download the program less than 1000? is it?