Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN, TMS570LS3137
Hello,
I am trying to communicate tms570ls1224 as MibSpi3 slave and when i send 8 16-bits from the master to the slave I see only the first word.
- I have TMS570LS12X Launchpad: Launchpad does not have MibSpi3 CS0 pin on the launchpad. Is CS0 pin must? If it is, is there any workaround?
- I have kept it as CS1 for now and the picture is my Halcogen Configuration for TG0. I am using TG0.
- I have configured SIMO,SOMI,CLK, CS1 as necessary pins functional with input/output.
- Are any of my configs wrong? Like Trigger events?
- What should I do to receive full 8 words from the master? The Master SPI would send all words in one transfer( meaning the CS is active for all the words
Thank you in advance.
Regards
Varun