Part Number: TMS570LS0432
Other Parts Discussed in Thread: LAUNCHXL-TMS57004, , HALCOGEN
Hello.
I am using two LAUNCHXL-TMS57004 launchpads (TMS570LS0432) and want to communicate between them using CAN. I am following the instructions as given in this Hercules CAN tutorial: https://training.ti.com/hercules-how-tutorial-can-communication
I have a few queries regarding the hardware connections:-
1) Without a transceiver, is it possible to communicate by connecting the CAN1TX to the CAN2RX of the same launchpad (it has two CAN ports)?
2) Without a transceiver, is it possible to communicate by connecting the CAN1TX of one launchpad to the CAN1RX of the second launchpad?
The launchpads do not have inbuilt transceivers and hence I am asking these questions. Is it all at possible to test CAN communication without the transceivers?
Thank you in advance.
-
Kartik