Part Number: TMS570LS3137
Other Parts Discussed in Thread: MOTORWARE,
hi,
I programmed het to prodeuce 1.25 mhz clock on pin 13(by het.ide), in slave mode, can I physically connect this pin to mibspi clock input?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS3137
Other Parts Discussed in Thread: MOTORWARE,
hi,
I programmed het to prodeuce 1.25 mhz clock on pin 13(by het.ide), in slave mode, can I physically connect this pin to mibspi clock input?
Hi Miro,
Thanks for your response. My program reads data from a poition encoder with BİSS protocol interface. As I had written before, Clock required in BİSS protocol is produce by het. When encoder receives this clock, it sends instantaneous position data. I use mibspi1 and everything is ok, but I programmed mibspi1 in master mode to produce internal clocks only for receiving data, and SPICLK pin is not used phisically. In order to improve program performance I want to use salve mode with my het clock for receiving data also. So if, het pin can be assigned as external clock source, there would be no need to set mibspi in master mode, and only one clock source can give service, both to encoder and mibspi receive mechanism. All these are inserted in motorware program, but when SPICLK is used as clock source, BLDC begins to vibrating and I couldn’t find the reason (may be a hardware problem), but CLOCK produced by het with the same frequency as mibspi clock (1.25Mhz) works very well and there is no vibration.
Best Regards
Ali Riza