Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
Hello,
I use the following program to read , average and print on screen values from an MPU6050 sensor
////////////////////////////////////////////////////////////////////////////////////////////////////
#include <stdbool.h>
#include <stdint.h>
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/pwm.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "inc/hw_gpio.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include <math.h>
#include <stddef.h> // For using the NULL pointer
#define PWM_FREQUENCY 55
////////////////////////////////////////////////////////////////////////////////////////////////////
// My I2C defines & includes
#include "driverlib/i2c.h"
#include "driverlib/interrupt.h"
#include "inc/hw_i2c.h"
#include "inc/hw_ints.h"
#include "sensorlib/i2cm_drv.h"
#include "sensorlib/mpu6050.h"
#include "sensorlib/hw_mpu6050.h"
#define DEBUG
////////////////////////////////////////////////////////////////////////////////////////////////////
// My UART defines & includes
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
////////////////////////////////////////////////////////////////////////////////////////////////////
#include "definitions_mpu6050.h"
tI2CMInstance g_sI2CInst; // I2C master driver structure. "tI2CMInstance" is defined in the i2cm_drv.h file.
tMPU6050 g_sMPU6050Inst; // MPU6050 sensor driver structure. "tMPU6050" is defined in the mpu6050.h file.
volatile unsigned long g_vui8DataFlag; // Data ready flag
volatile unsigned long g_vui8ErrorFlag; // Error flag
void
ISL29023I2CIntHandler(void)
{
I2CMIntHandler(&g_sI2CInst);
}
////////////////////////////////////////////////////////////////////////////////////////////////////
int main(void)
{
float fAccel[3], fGyro[3] = {0.0} ;
uint8_t register_mpu6050_o_pwr_mgmt_1 ; // Used for debug
uint8_t register_mpu6050_o_who_am_i ; // Used for debug
uint8_t index = 0 ;
uint32_t counter = 0 ;
int32_t i32IntegerPart = 0 ;
int32_t i32FractionPart = 0 ;
// Configure the clock
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
////////////////////////////////////////////////////////////////////////////////////////////////////
// My I2C initialization code
// Enable GPIO peripheral that contains I2C 2
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
// Enable I2C module 2
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C2);
// Configure the pin muxing for I2C2 functions on port E4 and E5.
GPIOPinConfigure(GPIO_PE4_I2C2SCL);
GPIOPinConfigure(GPIO_PE5_I2C2SDA);
// Select the I2C function for these pins.
GPIOPinTypeI2CSCL(GPIO_PORTE_BASE, GPIO_PIN_4);
GPIOPinTypeI2C(GPIO_PORTE_BASE, GPIO_PIN_5);
IntMasterEnable();
// USER_I2CMInit(&g_sI2CInst, I2C2_BASE, INT_I2C2, 0xFF, 0xFF, SysCtlClockGet()); // Set SCL to 100KHz instead of the original 400KHz.
I2CMInit(&g_sI2CInst, I2C2_BASE, INT_I2C2, 0xFF, 0xFF, SysCtlClockGet());
SysCtlDelay(SysCtlClockGet() / 3);
// USER_MPU6050Callback will modify the g_bMPU6050Done variable to true if the functions that use it succeed.
// Initialize the MPU6050
g_bMPU6050Done = false;
MPU6050Init(&g_sMPU6050Inst, &g_sI2CInst, MPU6050_I2C_ADDRESS, USER_MPU6050Callback, 0);
while(!g_bMPU6050Done) { }
// SysCtlDelay(SysCtlClockGet() / 3);
g_bMPU6050Done = false;
MPU6050Read(&g_sMPU6050Inst, MPU6050_O_WHO_AM_I , ®ister_mpu6050_o_who_am_i, 1 ,USER_MPU6050Callback , 0);
while(!g_bMPU6050Done) { }
SysCtlDelay(SysCtlClockGet() / 3);
g_bMPU6050Done = false;
MPU6050Read(&g_sMPU6050Inst, MPU6050_O_PWR_MGMT_1 , ®ister_mpu6050_o_pwr_mgmt_1, 1 ,USER_MPU6050Callback , 0); // Someone forgot to take the device out of sleep.
while(!g_bMPU6050Done) { }
SysCtlDelay(SysCtlClockGet() / 3);
g_bMPU6050Done = false;
// Writing 0x01 wakes up the device from sleep and also makes the main clock PLL with X axis gyroscope reference.
MPU6050Write(&g_sMPU6050Inst, MPU6050_O_PWR_MGMT_1 , 0x01 , 1 , USER_MPU6050Callback , 0);
while(!g_bMPU6050Done) { }
SysCtlDelay(SysCtlClockGet() / 3);
g_bMPU6050Done = false;
MPU6050Read(&g_sMPU6050Inst, MPU6050_O_PWR_MGMT_1 , ®ister_mpu6050_o_pwr_mgmt_1 , 1 ,USER_MPU6050Callback , 0);
while(!g_bMPU6050Done) { }
SysCtlDelay(SysCtlClockGet() / 3);
g_bMPU6050Done = false;
// Configure the MPU6050 for +/- 4 g accelerometer range.
MPU6050ReadModifyWrite(&g_sMPU6050Inst, MPU6050_O_ACCEL_CONFIG, ~MPU6050_ACCEL_CONFIG_AFS_SEL_M, MPU6050_ACCEL_CONFIG_AFS_SEL_2G, USER_MPU6050Callback, 0);
while(!g_bMPU6050Done) { }
SysCtlDelay(SysCtlClockGet() / 3);
////////////////////////////////////////////////////////////////////////////////////////////////////
// My UART initialization code
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
UARTStdioConfig(0, 115200, 16000000);
UARTprintf("The UART Works\n");
while(1)
{
g_bMPU6050Done = false;
while ( counter < 1000000 )
{
counter ++ ;
}
counter = 0 ;
// Get the new accelerometer and gyroscope readings.
// MPU6050DataAccelGetFloat(&g_sMPU6050Inst, &fAccel[0], &fAccel[1], &fAccel[2]);
// MPU6050DataGyroGetFloat(&g_sMPU6050Inst, &fGyro[0], &fGyro[1], &fGyro[2]);
sample_accumulate_average
(
&g_sMPU6050Inst ,
8 ,
fAccel ,
fGyro
) ;
// Convert floating point to an integer and send it via UART
for ( index = 0 ; index <= 2 ; index ++ )
{
i32IntegerPart = (int32_t)fAccel[index];
i32FractionPart = (int32_t)(fAccel[index] * 1000.0f);
i32FractionPart = i32FractionPart - (i32IntegerPart * 1000);
if(i32FractionPart < 0)
{
i32FractionPart *= -1;
}
if ( index == 0 )
{
UARTprintf("Accelerometer X: %3d.%03d\t\n", i32IntegerPart, i32FractionPart);
}
if ( index == 1 )
{
UARTprintf("Accelerometer Y: %3d.%03d\t\n", i32IntegerPart, i32FractionPart);
}
if ( index == 2 )
{
UARTprintf("Accelerometer Z: %3d.%03d\t\n", i32IntegerPart, i32FractionPart);
}
}
for ( index = 0 ; index <= 2 ; index ++ )
{
i32IntegerPart = (int32_t)fGyro[index];
i32FractionPart = (int32_t)(fGyro[index] * 1000.0f);
i32FractionPart = i32FractionPart - (i32IntegerPart * 1000);
if(i32FractionPart < 0)
{
i32FractionPart *= -1;
}
if ( index == 0 )
{
UARTprintf("Gyro X: %3d.%03d\t\n", i32IntegerPart, i32FractionPart);
}
if ( index == 1 )
{
UARTprintf("Gyro Y: %3d.%03d\t\n", i32IntegerPart, i32FractionPart);
}
if ( index == 2 )
{
UARTprintf("Gyro Z: %3d.%03d\t\n\n\n\n\n", i32IntegerPart, i32FractionPart);
}
}
// Clear the accumulated values to prepare for a new cycle.
fAccel[0] = 0.0 ;
fAccel[1] = 0.0 ;
fAccel[2] = 0.0 ;
fGyro[0] = 0.0 ;
fGyro[1] = 0.0 ;
fGyro[2] = 0.0 ;
}
}
Here is the code for the "sample_accumulate_average" function
void sample_accumulate_average ( tMPU6050 * g_sMPU6050Inst , int number_of_samples , float *accelerometer_average , float *gyro_average) // the function receives as an argument pointer to arrays of 3 elements
{
float accelerometer_reading[3], gyro_reading[3] = {0.0};
int sample_counter ;
int axis_number ;
for ( sample_counter = 0 ; sample_counter < number_of_samples ; sample_counter ++ )
{
MPU6050DataRead(g_sMPU6050Inst, USER_MPU6050Callback, 0);
while(!g_bMPU6050Done) { }
MPU6050DataAccelGetFloat(g_sMPU6050Inst, &accelerometer_reading[0], &accelerometer_reading[1], &accelerometer_reading[2]);
MPU6050DataGyroGetFloat(g_sMPU6050Inst, &gyro_reading[0], &gyro_reading[1], &gyro_reading[2]);
for ( axis_number = 0 ; axis_number < 3 ; axis_number ++ )
{
accelerometer_average [ axis_number ] = accelerometer_average [ axis_number ] + accelerometer_reading [ axis_number ] ; // accumulate accelerometer readings
gyro_average [ axis_number ] = gyro_average [ axis_number ] + gyro_reading [ axis_number ] ; // accumulate gyro readings
}
}
for ( axis_number = 0 ; axis_number < 3 ; axis_number ++ )
{
accelerometer_average [ axis_number ] = accelerometer_average [ axis_number ] / number_of_samples ;
gyro_average [ axis_number ] = gyro_average [ axis_number ] / number_of_samples ;
}
}
The program runs and prints values on the screen. But it's VERY sensitive to the number of samples that I choose to average (8 in the above code).
When I set the value to 1 (no averaging) - correct values appear.
When I increase the value (to induce averaging) - for example to 8. Erroneous values are printed.
I think it has something to do with the fact that I'm using floats and accumulate them - perhaps an overflow of some kind.
What do you think ?