Other Parts Discussed in Thread: MSP-FET
Tool/software: Code Composer Studio
Sir, I am using cc430f6137 ic. my doubt is,
1. what is maximum input voltage apply to adc input channels.
2.the current sensor which i am using is very sensitive, the output rating will be (13.33mV) for each amperes.
3.the ADC output value from the MCU is varies between 10 to 20mV and above. so I can't capture accurate value of sensor.
4.I am using this (cc430x613x_adc12_07) sample adc code and this value is monitor through uart communication. I am using single sensor only.
5.Do you have any other suggestion to use alternate adc code (or) i can use same adc code to achieve accuracy.
6.what are the possibilities and options should be done in my code(cc430x613x_adc12_07).
Please send soon,
Regards by,
Siva.E