Part Number: TMS570LC4357
Hello,
We are currently using the TMS570LC4357 and we have some questions about the IOMM function.
- We do not find the information about the behaviour when signal or terminal is configurable both by the input multiplexing and the output multiplexing.Could you tell us more about this ?
- Since there is a default value on Input and Output multiplexing (i.e. IOMM always activated):
What the the behaviour if we use a pin as output (configured via output multiplexing) whereas the pin is also configurable via input multiplexing?
What the the behaviour if we use a pin as input (configured via input multiplexing) whereas the pin is also configurable via output multiplexing?
- Since there is a default value on Input and Output multiplexing (i.e. IOMM always activated),
what is the behaviour in the IOMM module if a pin configurable via input ou output multiplexing is used as GIO ?
Is the IOMM configuration performed once the pin is in GIO mode ?
Best regards,
Christopher