This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TM4C1230E6PM: FaultISR interrupt on Tiva-c TM4C123

Part Number: TM4C1230E6PM


Tool/software: TI C/C++ Compiler

I have a simple question, My program is trapped at Fault ISR,

Below is my code that is trapped at Fault ISR

int writeProgMemoryBlock(const unsigned char *data, uint16_t dataSize, uint8_t bank, uint8_t address, int verify) {
    //return writeMemoryBlock(data, dataSize, bank, address, verify, 1);
        setMemoryBank(bank,0,0);
        setMemoryStartAddress(address);
        uint8_t chunkSize;
        uint8_t *verifyBuffer;
        uint8_t *progBuffer;
        uint16_t i;
        uint8_t j;
        if (verify) verifyBuffer = (uint8_t *)malloc(MPU6050_DMP_MEMORY_CHUNK_SIZE);
        if (1) progBuffer = (uint8_t *)malloc(MPU6050_DMP_MEMORY_CHUNK_SIZE);
        for (i = 0; i < dataSize;) {
            // determine correct chunk size according to bank position and data size
            chunkSize = MPU6050_DMP_MEMORY_CHUNK_SIZE;

            // make sure we don't go past the data size
            if (i + chunkSize > dataSize)
                chunkSize = dataSize - i;

            // make sure this chunk doesn't go past the bank boundary (256 bytes)
            if (chunkSize > 256 - address)
                chunkSize = 256 - address;

            if (1) {
                // write the chunk of data as specified
                for (j = 0; j < chunkSize; j++) progBuffer[j] = pgm_read_byte(data + i + j);
            } else {
                // write the chunk of data as specified
                progBuffer = (uint8_t *)data + i;
            }

             for (i = 0; 0 < chunkSize; i++){
                 writeByte(devAddr, MPU6050_RA_MEM_R_W, progBuffer[i]);
             }




            // verify data if needed
            if (verify && verifyBuffer) {
                setMemoryBank(bank,0,0);
                setMemoryStartAddress(address);
                readBytes(devAddr, MPU6050_RA_MEM_R_W, chunkSize, verifyBuffer);
                if (memcmp(progBuffer, verifyBuffer, chunkSize) != 0) {

                    free(verifyBuffer);
                    if (1) free(progBuffer);
                    return false; // uh oh.
                }
            }

            // increase byte index by [chunkSize]
            i += chunkSize;

            // uint8_t automatically wraps to 0 at 256
            address += chunkSize;

            // if we aren't done, update bank (if necessary) and address
            if (i < dataSize) {
                if (address == 0) bank++;
                setMemoryBank(bank,0,0);
                setMemoryStartAddress(address);
            }
        }
        if (verify) free(verifyBuffer);
        if (1) free(progBuffer);
        return true;
} 

When I try to debug to go into the this function, it jumps into FaultISR function.

How to figure out the reason and solution of the problem?

I use code composer studio with TM4C123. I am trying to read quaternion values from MPU6050. I finished my code but I couldn't finalize my project.

Thanks in advance