Part Number: TMS570LS1114
Tool/software: Code Composer Studio
Hi Team,
I have a customer with the following question about the TMS570LS1114
we are using a system with an OS including memory protection. If the memory protection is active, the F021 Flash API execution is aborted by exception. The flash api library is called in a OS task that runs in user mode. The MPU allows RW access to “Bank 7 0xF020_0000 0xF03F_FFFF” and “Flash Module 0xFFF8_7000 - 0xFFF8_7FFF”.
The controller TMS570LS1114 is used.
Which address range are used by the F021 Flash Api?
Which registers are used by the F021 Flash Api?
What can we do read, to write and to erase the data flash (flash bank 7) when the code is executed in user mode?
Regards
Mihir