Part Number: TMS570LC4357
Hello,
We would like to have more information about EMAC deactivation means.
The Reference manual mention in section 32.2.15.1 that "Unlike the EMAC module, the MDIO and EMAC control modules cannot be placed in reset from a register inside their memory map."
Nevertheless the EMAC control module seems to be in reset via the RESET bit in the SOFTRESET register (section 32.3.2) whereas the EMAC module is in reset via the SOFTRESET bit in the SOFTRESET register (section 32.5.34).
Could you precise us if each of these modules can be reset via the registers as described in registers section of reference manual ?
Best regards,
Christopher