Part Number: TMS570LS3137
In AUTOSAR_MCAL_TMS570LSx-05.30.00, the Range for McuClockReferencePointFrequency is [5000000; 20000000]Hz. We need to use the Frequency referency for values beyond this range of 5MHz - 20MHz. The AUTOSAR specification ( AUTOSAR_SWS_MCUDriver.pdf - Parameter McuClockReferencePoint) does not provide such a limitation and the Range is [0 .. INF].
Can this range be extended atleast till 100MHz?
UseCase:
This McuClockReferencePoint is used to specify the LIN Clock reference which is VCLK and the value will be in the order of 80MHz for this project.