Part Number: TMS570LC4357
Hello,
We would like to have more information about N2HET.
As described in the Referendce manual (Figure 23-1.) the N2HET modules can be turn off via the TO bit in the HETGCR register.
But does it mean that all the module is in 'reset state' (GIO functionality included) ?
Is there a means to deactivate the GIO functionality of the N2HET module at the same time the N2HET 'core' of the N2HET module?
Compared to some other modules, It seems that no choice can be done between N2HET functionality and GIO functionality for N2HET pins.
Best regards,
Christopher