Part Number: TM4C1290NCPDT
Hello,
I am using TI-RTOS Drivers to UART. (TI-RTOS 2.16)
I want to change Interrupt FIFO Level Select.
I have tried UARTFIFOLevelSet API after UART_open().
my code:
//RTOS UART Drivers
UART_Params uart_params;
UART_Params_init(uart_params);
up->baudRate = 500000; //boudrate 500kbps
up->readDataMode = UART_DATA_BINARY;
up->writeDataMode = UART_DATA_BINARY;
up->readReturnMode = UART_RETURN_FULL;
up->readEcho = UART_ECHO_OFF;
up->readTimeout = 100;
uart = UART_open(Board_UART6, &uart_params);
//Peripheral Driver Library UART API.
// UARTIFLS register is Interrupt FIFO Level Select.
// RX FIFO 1/8 to 1/2(UART_FIFO_RX4_8)
UARTFIFOLevelSet(UART6_BASE, UART_FIFO_TX1_8, UART_FIFO_RX4_8);
The result showed that UARTIFLS(UART6 UARTIFLS:0x40012034) register value changes 0x00000000 to 0x00000010.
Is this the right approach?
Or is there another right way?
Thanks.