Part Number: TMS570LS0432
Tool/software: Code Composer Studio
Hi,
Recently I have been trying to develop a bootloader for the TMS570. I can get the CAN communication working and can get said communication to save to Bank 7 using the FEE driver however, whenever I attempt to use the F021 API Fapi functions outside of the FEE driver I get an undefentry interrupt called followed by an error saying that the function document cannot be found.
I have linked the API properly using the appropriate linker library however, no matter what I do I always get the same error even when I attempt to initialize the Fapi Bank.
Any help would be greatly appreciated.
Here is my code used for the flash writing I'd like to do:
uint32_t Fapi_UpdateStatusProgram( uint32_t Bank, uint32_t Flash_Start_Address, uint32_t Data_Start_Address, uint32_t Size_In_Bytes)
{
register uint32_t src = Data_Start_Address;
register uint32_t dst = Flash_Start_Address;
unsigned int bytes, status = 0;
Fapi_StatusType oReturnCheck = Fapi_Status_Success;
if (Size_In_Bytes < 16)
bytes = Size_In_Bytes;
else
bytes = 16;
Fapi_initializeAPI((Fapi_FmcRegistersType *)F021_CPU0_REGISTER_ADDRESS, (uint32_t)SYS_CLK_FREQ);
oReturnCheck= Fapi_initializeFlashBanks(10); //10Mhz
if((oReturnCheck == Fapi_Status_Success)){
oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank0);
//while(FLASH_CONTROL_REGISTER->FmStat.FMSTAT_BITS.Busy == Fapi_Status_FsmBusy);
delay();
}
//delay();
Fapi_setActiveFlashBank((Fapi_FlashBankType)0);
Fapi_issueProgrammingCommand((uint32_t *)dst,
(uint8_t *)src,
(uint32_t) bytes, //8,
0,
0,
Fapi_AutoEccGeneration);
while( Fapi_checkFsmForReady() == Fapi_Status_FsmBusy );
status = Flash_Program_Check(Flash_Start_Address, Data_Start_Address, Size_In_Bytes);
delay();
return (status);
}
Thanks,
Ron Haber