Hi, Any special developments boards instead of Raspberry Pi which can receive the wireless mesh network data via ZigBee devices?
We are using a mesh network with 5 poly house situated nearby field area of 700 meters away from each other.
We want to receive and grab all the data from the wireless temperature sensor which uses the ZigBee device for wireless communication so I need a station hardware which receives the data from the access point nodes and at the same time send the data to the internet cloud.
any suggestion regarding this will be a great help.