Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
HI,
Attached
/** @file sys_main.c
* @brief Application main file
* @date 07-July-2017
* @version 04.07.00
*
* This file contains an empty main function,
* which can be used for the application.
*/
/*
* Copyright (C) 2009-2016 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* USER CODE BEGIN (0) */
#include "can.h"
#include "gio.h"
#include"stdint.h"
/* USER CODE END */
/* Include Files */
#include "sys_common.h"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
uint32_t a,b;
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
uint8 data[8]={0x11,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
canInit();
gioInit();
//canUpdateID(canREG1, canMESSAGE_BOX1, 0x00000200U);
a=canGetID(canREG1,canMESSAGE_BOX1);
while(1)
{
b= canTransmit(canREG1, canMESSAGE_BOX1,data);
//canTransmit(canREG1, 0x120,x);
gioSetBit(gioPORTB, 1, 1);
}
/* USER CODE END */
return 0;
}
/* USER CODE BEGIN (4) */
//uint32_t TX_std_ID(uint32_t eleven_bit)
//{
// if (eleven_bit>0x7ff)
// {
// eleven_bit=0x7ff;
// }
//
// 0x0A000000 || 0x7ff;
//}
//void canMessageNotification(canBASE_t *node, uint32_t messageBox)
//{
// return;
//}
//
//
//void canErrorNotification(canBASE_t *node, uint32_t notification)
//{
// return;
//}
//
//void esmGroup1Notification(unsigned channel)
//{
// return;
//}
//
//void esmGroup2Notification(unsigned channel)
//{
// return;
//}
/* USER CODE END */
is my sys_main.c file
I am able to send 200 ID over CAN.
if i uncomment the following line to change the ID to hex 210 (line no. 81)
//canUpdateID(canREG1, canMESSAGE_BOX1, 0x00000210U);
No message is sent over CAN.
Help me in changing the ID in code using halcogen generated function. i dont want to mess up the generated code.
Thanks.