This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEMU110-U: TMS570LS0432 Isolation

Part Number: TMDSEMU110-U
Other Parts Discussed in Thread: TMS570LS0432

Hello.

I am using the TMDSEMU110-U Debugger for my Hercules TMS570LS0432 MCU. I had the following queries:-

1) Is there inbuilt isolation for this device?

2) If not, is a version of this device with isolation, availble?

Thanks in advance.

-

Kartik

  • Hello Kartik,

    There is no isolation on the TMDSEMU110-U debug pod.

    You could create an isolation adapter, or place the isolation on your application board. You can use 2 isolation chips such as ISO7240 and ISO7231 to isolate TDO/TDI/TCK signals.