Hello,
We would like to have more information about N2HET.
As described in the Referendce manual (Figure 23-1.) the N2HET modules can be turn off via the TO bit in the HETGCR register.
GIO functionality of N2HET module seems cannot be turned off.
Is it possible to put the N2HET pins in N2HET functionality rather GIO functionality (in order to cut-off the GIO functionality) ?
Or is there another means to shut-off the N2HET that TO bit to stop globally the NHET ?
Is the HETPINDIS, the good register to disable the N2HET pins ?
E.g :
- Pin disabled if HETPINDIS at 0x00 + HETDIR at 0x00
- Output buffer disabled (Hi-Z) if HETPINDIS at 0x01 and (nDIS at 0x00 or HETDIR at 0x00 or HET Pin ENA at 0x00)
Best regards,
Christopher