Other Parts Discussed in Thread: TMS470R1B1M
Hi guys
Here is a example code in which the timer is used to trigger the ADC at 10 ms. I've run this code and the clock is right 10ms. However, i dont know how to obtain this clock, as LR Div = 8, HR Div = 10 and SYSCLK = 58.9824MHz. In my opinion, the clock for interrupt should be calculated by SYSCLK /(LRDIV * HRDIV) = 59MHz / 80. How does 10ms come from?
Thanks a lot
Here is the code
#include <intrinsic.h>
#include "iotms470r1b1m.h"
#include "tms470r1b1m_bit_definitions.h"
#include "std_het.h"
#include "tms470r1b1m_HET_INT_02_H.h"
void MemCopy32(unsigned long *dst, unsigned long *src, int bytes);
__no_init volatile HETPROGRAM0_UN e_HETPROGRAM0_UN @ 0x00800000;
volatile unsigned int result[20];
unsigned int average;
void main(void)
{
PCR = CLKDIV_3; // ICLK = SYSCLK / 3
GCR = ZPLL_CLK_DIV_PRE_1; // SYSCLK = 8 x fOSC
PCR |= PENABLE; // Enable peripherals
REQMASK = 0; // clear interrupt mask
REQMASK |= (1<<CIM_MIBADCE1); // enable channel 27 (AD1)
ADCR1 |= PS_8; // ADCLK prescaler = 8
ADSAMPEV |= SEN; // ADCSAMP1 controls SW
ADSAMP1 = 62; // SW = 62+2
ADCR1 |= ADC_EN; // Enable ADC
ADISR1 = 0x0001; // group 1 = channel 0
ADEVTSRC = G1_SRC_INT1 + G1_EDG_SEL + G1_ENA; // enable group 1 and set trigger for low
// to high transition
ADBCR1 |= BUF_EN; // enable buffered mode
ADBCR1 |= BNDA_8; // set RAM boundary between event and group 1
// units of two words from the beginning of buffer
// event group has 8*2 = 16 words for the FIFO
ADBCR1 |= BNDB_16 + BNDB_2; // set RAM boundary between group 1 and 2
// units of two words from the beginning of buffer
// group 1 has (18-8)*2 = 20 words for the FIFO
ADBCR2 |= BNDEND_64; // set RAM buffer end boundary
// 64-word FIFO buffer
// group 2 has 64-(2*18) = 28 words for the FIFO
ADTHRG1 = G1THR_16 + G1THR_4; // group 1 threshold counter = 20, 20 results will be
// placed on the buffer before setting G1 BUF INT FLAG
ADBUFST &= ~G1_INT_FLAG; // clear flag
ADBCR3 |= G1_OVR_INT_EN; // enable group 1 FIFO buffer over-run interrupt
ADBCR3 |= G1_BUF_INT_EN; // enable group 1 FIFO buffer interrupt
HETGCR = CLK_MASTER + IGNORE_SUSPEND; // HET Master Mode, Ignore SW BP
// Copy HET instructions to HET RAM
MemCopy32((void *)&e_HETPROGRAM0_UN, (void *)HET_INIT0_PST,
sizeof(HET_INIT0_PST));
HETPFR = 0x00000309; // Set LR Div = 8, HR Div = 10
HETDCLR = 0xffffffff; // Clear HET output latches
HETDIR = 0xffffffff; // Set HET as GIO outputs
HETGCR |= ON; // Start HET
__enable_interrupt(); // enable interrupts
while (1); // Loop forever...
}
//------------------------------------------------------------------------------
// This module programms the HET RAM with the HET code
//------------------------------------------------------------------------------
void MemCopy32(unsigned long *dst, unsigned long *src, int bytes)
{
for (int i = 0; i < (bytes + 3) / 4; i++)
*dst++ = *src++;
}
//------------------------------------------------------------------------------
// TMS470R1B1M Standard Interrupt Handler
//------------------------------------------------------------------------------
__irq __arm void irq_handler(void)
{
switch ((0xff & IRQIVEC)-1)
{
case CIM_MIBADCE1 : // channel 27 (AD1) interrupt?
if (ADBUFST & 0x0020) // buffer over-run?
{
ADISR1 = 0x0001; // clear buffer
ADTHRG1 = G1THR_16 + G1THR_4; // reset group 1 threshold
}
else
{
unsigned int i;
ADBUFST &= ~G1_INT_FLAG; // clear flag
average = 0;
for (i=0; i<20; i++)
{
result[i] = ADBUF1; // read FIFO value
average = average + result[i]; // sum values
}
average = (unsigned int) average / 20; // get average
HETDOUT = average & 0xff; // Output 8 LSBs to LEDs
}
break;
}
}