Part Number: TMS570LS3137
I have a bootloader in my project, so I am updating the image during run-time. I have a reproducible scenario where post-new code load, the first call to Fapi_initializeFlashBanks will corrupt (at least one) file-scope variable (that was already initialized).
I saw a prior post that the API-source was unavailable. If that is still true, can I get the source to Fapi_initializeFlashBanks?
If I cannot get the function or API source, can you tell me about global / file-scope variables Fapi_initializeFlashBanks is using -- where in memory are they stored, and can I see them in the map-file?
Also is Fapi_initializeFlashBanks using linker-generated pointer-constants (like __TI_PINIT_Base)?
Something in Fapi_initializeFlashBanks is not being updated properly after writing a new flash-image (during run-time).
Thanks,
Jim