This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TM4C123GH6PM: "boot_demo1" not working while calling interrupt in it.

Part Number: TM4C123GH6PM

Tool/software: TI C/C++ Compiler

I am facing the same problem,code does not work when i call UART0 interrupt in code "boot_demo1" it stopped working, without interrupt,code is working fine.

code have problem in callingROM_IntEnable(UART0_BASE);

without calling interrupt code is woking fine.

//*****************************************************************************
//
// boot_demo1.c - First boot loader example.
//
// Copyright (c) 2012-2017 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
// 
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
// 
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
// 
// This is part of revision 2.1.4.178 of the DK-TM4C123G Firmware Package.
//
//*****************************************************************************

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_flash.h"
#include "inc/hw_memmap.h"
#include "inc/hw_sysctl.h"
#include "inc/hw_gpio.h"
#include "inc/hw_nvic.h"
#include "inc/hw_types.h"
#include "driverlib/pin_map.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/sysctl.h"
#include "driverlib/flash.h"
#include "driverlib/interrupt.h"
#include "driverlib/uart.h"
#include "driverlib/rom.h"
#include "utils/ustdlib.h"
#include "grlib/grlib.h"
#include "drivers/cfal96x64x16.h"

uint8_t ui8PinData=2;
int gtch=0;
int getpin=0;
//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Boot Loader Demo 1 (boot_demo1)</h1>
//!
//! An example to demonstrate the use of a flash-based boot loader. At
//! startup, the application will configure the UART and USB peripherals,
//! and then branch to the boot loader to await the start of an
//! update. If using the serial boot loader (boot_serial), the UART will
//! always be configured at 115,200 baud and does not require the use of
//! auto-bauding.
//!
//! This application is intended for use with any of the three flash-based boot
//! loader flavors (boot_serial or boot_usb) included in the software
//! release. To accommodate the largest of these (boot_usb), the link address
//! is set to 0x2800. If you are using serial, you may change this
//! address to a 1KB boundary higher than the last address occupied
//! by the boot loader binary as long as you also rebuild the boot
//! loader itself after modifying its bl_config.h file to set APP_START_ADDRESS
//! to the same value.
//!
//! The boot_demo2 application can be used along with this application to
//! easily demonstrate that the boot loader is actually updating the on-chip
//! flash.
//!
//! Note that the TM4C123G and other Blizzard-class devices also
//! support the serial and USB boot loaders in ROM. To make use of this
//! function, link your application to run at address 0x0000 in flash and enter
//! the bootloader using the ROM_UpdateSerial and ROM_UpdateUSB functions 
//! (defined in rom.h). This mechanism is used in the utils/swupdate.c 
//! module when built specifically targeting a suitable Blizzard-class device.
//
//*****************************************************************************

//*****************************************************************************
//
// Graphics context used to show text on the CSTN display.
//
//*****************************************************************************
tContext g_sContext;

//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

//*****************************************************************************
//
// Passes control to the bootloader and initiates a remote software update.
//
// This function passes control to the bootloader and initiates an update of
// the main application firmware image via UART0 or USB depending
// upon the specific boot loader binary in use.
//
// \return Never returns.
//
//*****************************************************************************
void
JumpToBootLoader(void)
{
//
// Disable all processor interrupts. Instead of disabling them
// one at a time, a direct write to NVIC is done to disable all
// peripheral interrupts.
//
HWREG(NVIC_DIS0) = 0xffffffff;
HWREG(NVIC_DIS1) = 0xffffffff;

//
// Return control to the boot loader. This is a call to the SVC
// handler in the boot loader.
//
(*((void (*)(void))(*(uint32_t *)0x2c)))();
}

//*****************************************************************************
//
// Initialize UART0 and set the appropriate communication parameters.
//
//*****************************************************************************
void
SetupForUART(void)
{
//
// We need to make sure that UART0 and its associated GPIO port are
// enabled before we pass control to the boot loader. The serial boot
// loader does not enable or configure these peripherals for us if we
// enter it via its SVC vector.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);

//
// Set GPIO A0 and A1 as UART.
//
ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);

//
// Configure the UART for 115200, n, 8, 1
//
ROM_UARTConfigSetExpClk(UART0_BASE, SysCtlClockGet(), 115200,
(UART_CONFIG_PAR_NONE | UART_CONFIG_STOP_ONE |
UART_CONFIG_WLEN_8));

//
// Enable the UART operation.
//
ROM_UARTEnable(UART0_BASE);
ROM_UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT); //only enable RX and TX interrupts
ROM_IntEnable(UART0_BASE); //enable the UART interrupt
ROM_IntMasterEnable();
}

//*****************************************************************************
//
// Enable the USB controller
//
//*****************************************************************************
void
SetupForUSB(void)
{
//
// The USB boot loader takes care of all required USB initialization so,
// if the application itself doesn't need to use the USB controller, we
// don't actually need to enable it here. The only requirement imposed by
// the USB boot loader is that the system clock is running from the PLL
// when the boot loader is entered.
//
}

//ENABLE LED
void Setup_LED(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
GPIOPinTypeGPIOInput(GPIO_PORTF_BASE, GPIO_PIN_4);
GPIOPadConfigSet(GPIO_PORTF_BASE,GPIO_PIN_4,GPIO_STRENGTH_2MA,GPIO_PIN_TYPE_STD_WPU);
}
//*****************************************************************************
//
// Demonstrate the use of the boot loader.
//
//*****************************************************************************
int
main(void)
{
// tRectangle sRect;
// tContext sContext;

//
// Enable lazy stacking for interrupt handlers. This allows floating-point
// instructions to be used within interrupt handlers, but at the expense of
// extra stack usage.
//
// ROM_FPULazyStackingEnable();

//
// Set the system clock to run at 50MHz from the PLL
//
SysCtlClockSet(SYSCTL_SYSDIV_2_5 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_MAIN);

//
// Initialize the peripherals that each of the boot loader flavors
// supports. Since this example is intended for use with any of the
// boot loaders and we don't know which is actually in use, we cover all
// bases and initialize for serial and USB use here.
//

// SetupForUSB();
Setup_LED();
SetupForUART();
// SetupForUART();
// Initialize the display driver.
//
// CFAL96x64x16Init();

//
// Initialize the graphics context.
//
// GrContextInit(&sContext, &g_sCFAL96x64x16);

//
// Fill the top part of the screen with blue to create the banner.
//
// sRect.i16XMin = 0;
// sRect.i16YMin = 0;
// sRect.i16XMax = GrContextDpyWidthGet(&sContext) - 1;
// sRect.i16YMax = 9;
// GrContextForegroundSet(&sContext, ClrDarkBlue);
// GrRectFill(&sContext, &sRect);

//
// Change foreground for white text.
//
// GrContextForegroundSet(&sContext, ClrWhite);

//
// Put the application name in the middle of the banner.
//
// GrContextFontSet(&sContext, g_psFontFixed6x8);
// GrStringDrawCentered(&sContext, "boot-demo1", -1,
// GrContextDpyWidthGet(&sContext) / 2, 4, 0);

//
// Indicate what is happening.
//
// GrStringDrawCentered(&sContext, "The boot loader", -1,
// GrContextDpyWidthGet(&sContext) / 2, 20, false);
// GrStringDrawCentered(&sContext, "is now running", -1,
// GrContextDpyWidthGet(&sContext) / 2, 30, false);
// GrStringDrawCentered(&sContext, "and awaiting", -1,
// GrContextDpyWidthGet(&sContext) / 2, 40, false);
// GrStringDrawCentered(&sContext, "an update.", -1,
// GrContextDpyWidthGet(&sContext) / 2, 50, false);

//
// Pass control to whichever flavor of boot loader the board is configured
// with.
//
// JumpToBootLoader();

//
// The previous function never returns but we need to stick in a return
// code here to keep the compiler from generating a warning.
//
// return(0);
while(1)
{
getpin = GPIOPinRead(GPIO_PORTF_BASE,GPIO_PIN_4); //PA6
if(getpin<=0)
{
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1| GPIO_PIN_2| GPIO_PIN_3, ui8PinData);
SysCtlDelay(10000000);
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x00);
SysCtlDelay(10000000);
JumpToBootLoader();
if(ui8PinData==8) {ui8PinData=2;} else {ui8PinData=ui8PinData*2;}


}
else
{
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1| GPIO_PIN_2| GPIO_PIN_3, ui8PinData);
SysCtlDelay(1000000);
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x00);
SysCtlDelay(1000000);
if(ui8PinData==8) {ui8PinData=2;} else {ui8PinData=ui8PinData*2;}
}
//JumpToBootLoader();

}
}

void UART0IntHandler(void)
{

uint32_t ui32Status;
ui32Status = UARTIntStatus(UART0_BASE, true); //get interrupt status
UARTIntClear(UART0_BASE, ui32Status); //clear the asserted interrupts

while(UARTCharsAvail(UART0_BASE)) //loop while there are chars
{
gtch= UARTCharGet(UART0_BASE);
if(gtch==0x48)
{
UARTCharPut(UART0_BASE,0x59);
}


}
}

boot_demo1_ccs.cmd file

/******************************************************************************
*
* boot_demo1_ccs.cmd - CCS linker configuration file for boot_demo1.
*
* Copyright (c) 2012-2017 Texas Instruments Incorporated. All rights reserved.
* Software License Agreement
* 
* Texas Instruments (TI) is supplying this software for use solely and
* exclusively on TI's microcontroller products. The software is owned by
* TI and/or its suppliers, and is protected under applicable copyright
* laws. You may not combine this software with "viral" open-source
* software in order to form a larger program.
* 
* THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
* NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
* NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
* CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
* DAMAGES, FOR ANY REASON WHATSOEVER.
* 
* This is part of revision 2.1.4.178 of the DK-TM4C123G Firmware Package.
*
*****************************************************************************/

--retain=g_pfnVectors

/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M3_T_le_eabi.lib */

/* The starting address of the application. Normally the interrupt vectors */
/* must be located at the beginning of the application. */
//#define APP_BASE 0x00002800
#define APP_BASE 0x00002800
#define RAM_BASE 0x20000000

/* System memory map */

MEMORY
{
/* Application stored in and executes from internal flash */
FLASH (RX) : origin = APP_BASE, length = 0x0003d800
/* Application uses internal RAM for data */
SRAM (RWX) : origin = 0x20000000, length = 0x00008000
}

/* Section allocation in memory */

SECTIONS
{
.intvecs: > APP_BASE
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.init_array : > FLASH

.vtable : > RAM_BASE
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM
}

__STACK_TOP = __stack + 1024;

startup_ccs.c file

//*****************************************************************************
//
// startup_ccs.c - Startup code for use with TI's Code Composer Studio.
//
// Copyright (c) 2012-2017 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
// 
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
// 
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
// 
// This is part of revision 2.1.4.178 of the DK-TM4C123G Firmware Package.
//
//*****************************************************************************

#include <stdint.h>
#include "inc/hw_nvic.h"
#include "inc/hw_types.h"

//*****************************************************************************
//
// Forward declaration of the default fault handlers.
//
//*****************************************************************************
void ResetISR(void);
static void NmiSR(void);
static void FaultISR(void);
static void IntDefaultHandler(void);

//*****************************************************************************
//
// External declaration for the reset handler that is to be called when the
// processor is started
//
//*****************************************************************************
extern void _c_int00(void);
extern void UART0IntHandler(void);
//*****************************************************************************
//
// Linker variable that marks the top of the stack.
//
//*****************************************************************************
extern uint32_t __STACK_TOP;
//extern void UART0IntHandler(void);

//*****************************************************************************
//
// The vector table. Note that the proper constructs must be placed on this to
// ensure that it ends up at physical address 0x0000.0000 or at the start of
// the program if located at a start address other than 0.
//
//*****************************************************************************
#pragma DATA_SECTION(g_pfnVectors, ".intvecs")
void (* const g_pfnVectors[])(void) =
{
(void (*)(void))((uint32_t)&__STACK_TOP),
// The initial stack pointer
ResetISR, // The reset handler
NmiSR, // The NMI handler
FaultISR, // The hard fault handler
IntDefaultHandler, // The MPU fault handler
IntDefaultHandler, // The bus fault handler
IntDefaultHandler, // The usage fault handler
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
IntDefaultHandler, // SVCall handler
IntDefaultHandler, // Debug monitor handler
0, // Reserved
IntDefaultHandler, // The PendSV handler
IntDefaultHandler, // The SysTick handler
IntDefaultHandler, // GPIO Port A
IntDefaultHandler, // GPIO Port B
IntDefaultHandler, // GPIO Port C
IntDefaultHandler, // GPIO Port D
IntDefaultHandler, // GPIO Port E
UART0IntHandler, // UART0 Rx and Tx
IntDefaultHandler, // UART1 Rx and Tx
IntDefaultHandler, // SSI0 Rx and Tx
IntDefaultHandler, // I2C0 Master and Slave
IntDefaultHandler, // PWM Fault
IntDefaultHandler, // PWM Generator 0
IntDefaultHandler, // PWM Generator 1
IntDefaultHandler, // PWM Generator 2
IntDefaultHandler, // Quadrature Encoder 0
IntDefaultHandler, // ADC Sequence 0
IntDefaultHandler, // ADC Sequence 1
IntDefaultHandler, // ADC Sequence 2
IntDefaultHandler, // ADC Sequence 3
IntDefaultHandler, // Watchdog timer
IntDefaultHandler, // Timer 0 subtimer A
IntDefaultHandler, // Timer 0 subtimer B
IntDefaultHandler, // Timer 1 subtimer A
IntDefaultHandler, // Timer 1 subtimer B
IntDefaultHandler, // Timer 2 subtimer A
IntDefaultHandler, // Timer 2 subtimer B
IntDefaultHandler, // Analog Comparator 0
IntDefaultHandler, // Analog Comparator 1
IntDefaultHandler, // Analog Comparator 2
IntDefaultHandler, // System Control (PLL, OSC, BO)
IntDefaultHandler, // FLASH Control
IntDefaultHandler, // GPIO Port F
IntDefaultHandler, // GPIO Port G
IntDefaultHandler, // GPIO Port H
IntDefaultHandler, // UART2 Rx and Tx
IntDefaultHandler, // SSI1 Rx and Tx
IntDefaultHandler, // Timer 3 subtimer A
IntDefaultHandler, // Timer 3 subtimer B
IntDefaultHandler, // I2C1 Master and Slave
IntDefaultHandler, // Quadrature Encoder 1
IntDefaultHandler, // CAN0
IntDefaultHandler, // CAN1
0, // Reserved
0, // Reserved
IntDefaultHandler, // Hibernate
IntDefaultHandler, // USB0
IntDefaultHandler, // PWM Generator 3
IntDefaultHandler, // uDMA Software Transfer
IntDefaultHandler, // uDMA Error
IntDefaultHandler, // ADC1 Sequence 0
IntDefaultHandler, // ADC1 Sequence 1
IntDefaultHandler, // ADC1 Sequence 2
IntDefaultHandler, // ADC1 Sequence 3
0, // Reserved
0, // Reserved
IntDefaultHandler, // GPIO Port J
IntDefaultHandler, // GPIO Port K
IntDefaultHandler, // GPIO Port L
IntDefaultHandler, // SSI2 Rx and Tx
IntDefaultHandler, // SSI3 Rx and Tx
IntDefaultHandler, // UART3 Rx and Tx
IntDefaultHandler, // UART4 Rx and Tx
IntDefaultHandler, // UART5 Rx and Tx
IntDefaultHandler, // UART6 Rx and Tx
IntDefaultHandler, // UART7 Rx and Tx
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
IntDefaultHandler, // I2C2 Master and Slave
IntDefaultHandler, // I2C3 Master and Slave
IntDefaultHandler, // Timer 4 subtimer A
IntDefaultHandler, // Timer 4 subtimer B
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
IntDefaultHandler, // Timer 5 subtimer A
IntDefaultHandler, // Timer 5 subtimer B
IntDefaultHandler, // Wide Timer 0 subtimer A
IntDefaultHandler, // Wide Timer 0 subtimer B
IntDefaultHandler, // Wide Timer 1 subtimer A
IntDefaultHandler, // Wide Timer 1 subtimer B
IntDefaultHandler, // Wide Timer 2 subtimer A
IntDefaultHandler, // Wide Timer 2 subtimer B
IntDefaultHandler, // Wide Timer 3 subtimer A
IntDefaultHandler, // Wide Timer 3 subtimer B
IntDefaultHandler, // Wide Timer 4 subtimer A
IntDefaultHandler, // Wide Timer 4 subtimer B
IntDefaultHandler, // Wide Timer 5 subtimer A
IntDefaultHandler, // Wide Timer 5 subtimer B
IntDefaultHandler, // FPU
0, // Reserved
0, // Reserved
IntDefaultHandler, // I2C4 Master and Slave
IntDefaultHandler, // I2C5 Master and Slave
IntDefaultHandler, // GPIO Port M
IntDefaultHandler, // GPIO Port N
IntDefaultHandler, // Quadrature Encoder 2
0, // Reserved
0, // Reserved
IntDefaultHandler, // GPIO Port P (Summary or P0)
IntDefaultHandler, // GPIO Port P1
IntDefaultHandler, // GPIO Port P2
IntDefaultHandler, // GPIO Port P3
IntDefaultHandler, // GPIO Port P4
IntDefaultHandler, // GPIO Port P5
IntDefaultHandler, // GPIO Port P6
IntDefaultHandler, // GPIO Port P7
IntDefaultHandler, // GPIO Port Q (Summary or Q0)
IntDefaultHandler, // GPIO Port Q1
IntDefaultHandler, // GPIO Port Q2
IntDefaultHandler, // GPIO Port Q3
IntDefaultHandler, // GPIO Port Q4
IntDefaultHandler, // GPIO Port Q5
IntDefaultHandler, // GPIO Port Q6
IntDefaultHandler, // GPIO Port Q7
IntDefaultHandler, // GPIO Port R
IntDefaultHandler, // GPIO Port S
IntDefaultHandler, // PWM 1 Generator 0
IntDefaultHandler, // PWM 1 Generator 1
IntDefaultHandler, // PWM 1 Generator 2
IntDefaultHandler, // PWM 1 Generator 3
IntDefaultHandler, // PWM 1 Fault
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
0, // Reserved
IntDefaultHandler, // I2C6 Master and Slave
IntDefaultHandler, // I2C7 Master and Slave
IntDefaultHandler, // HIM Scan Matrix Keyboard 0
IntDefaultHandler, // One Wire 0
IntDefaultHandler, // Remote Temperature Sensor 0
IntDefaultHandler, // HIM PS/2 0
IntDefaultHandler, // HIM LED Sequencer 0
IntDefaultHandler, // HIM Consumer IR 0
IntDefaultHandler, // Power Regulator Bus 0
(void (*)(void))0xFF01FF02, // HEADER PREFIX 0
(void (*)(void))0xFF03FF04, // HEADER PREFIX 1
(void (*)(void))0xFFFFFFFF, // HEADER IMAGE LEN
(void (*)(void))0xFFFFFFFF, // HEADER CRC32
(void (*)(void))0xFFFFFFFF, // HEADER Reserved
(void (*)(void))0xFFFFFFFF, // HEADER Reserved
(void (*)(void))0xFFFFFFFF, // HEADER Reserved
(void (*)(void))0xFFFFFFFF // HEADER Reserved
};

//*****************************************************************************
//
// This is the code that gets called when the processor first starts execution
// following a reset event. Only the absolutely necessary set is performed,
// after which the application supplied entry() routine is called. Any fancy
// actions (such as making decisions based on the reset cause register, and
// resetting the bits in that register) are left solely in the hands of the
// application.
//
//*****************************************************************************
void
ResetISR(void)
{
//
// Jump to the CCS C initialization routine. This will enable the
// floating-point unit as well, so that does not need to be done here.
//
__asm(" .global _c_int00\n"
" b.w _c_int00");
}

//*****************************************************************************
//
// This is the code that gets called when the processor receives a NMI. This
// simply enters an infinite loop, preserving the system state for examination
// by a debugger.
//
//*****************************************************************************
static void
NmiSR(void)
{
//
// Enter an infinite loop.
//
while(1)
{
}
}

//*****************************************************************************
//
// This is the code that gets called when the processor receives a fault
// interrupt. This simply enters an infinite loop, preserving the system state
// for examination by a debugger.
//
//*****************************************************************************
static void
FaultISR(void)
{
//
// Enter an infinite loop.
//
while(1)
{
}
}

//*****************************************************************************
//
// This is the code that gets called when the processor receives an unexpected
// interrupt. This simply enters an infinite loop, preserving the system state
// for examination by a debugger.
//
//*****************************************************************************
static void
IntDefaultHandler(void)
{
//
// Go into an infinite loop.
//
while(1)
{
}
}

Do i need to change something else in code to call interrupts

How to resolve the problem please help.