Part Number: TM4C123GE6PM
Tool/software: Code Composer Studio
Hello, I am new to the domain of Embedded System and currently I am working on TM123G6PM.
There are two things which I intend to do as per my College Assignmment.
1) Generating a Pulse Train of 200KHz with a on-off period 400ms using Timer/PWM
2) Using the Generated signal and sampling it using the ADC under oversampling conditions (Sampling Rate around 600Khz). And then storing the converted values in a array and plot a graph of that array.