This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: TM4C1294NCPDT

Part Number: TM4C1294NCPDT


Dear,

We are using lwip 1.4.1 ported with version resale TivaWare_C_Series-2.1.4.178 utilizing Free RTOS

we use tcp server using RAM_RAW at size of 32KB. 

The App, sends each 10msec a buffer of 14KB.

after a while we encounter that the PBUF is out of memory (cant allocate the tcp_write return MEM_ERR)

we saw there were issues with PBUF free, and the corrections applied to tiva-tm4c129.c were taken and merge. 

the issues with the PBUF leak seems to be solved on the lwip 2.2017 at least what was stated.

Q:

1. can you post the latest  source file tiva-tm4c129.c with all the mentioned fixes applied to it? 

2. when are you planning to port the tiva-tm4c129.c to new lwip release ? 

3. any ideas how to overcome the pbuf leak ? 

added lwipopts.h

#define PBUF_POOL_SIZE 42//16 //1024
#define TCP_MSS 1460//1476
#define TCP_WND (3*TCP_MSS) //(2*TCP_MSS)
#define TCP_SND_BUF (32*1024) //65535
#define TCP_OVERSIZE TCP_MSS
#define TCP_SND_QUEUELEN 256 //128 //(2 * TCP_SND_BUF/TCP_MSS)
#define MEMP_NUM_TCP_SEG TCP_SND_QUEUELEN //200 //512

the sender task codes partial is :

if (tcp_sndbuf(pState->pConnectPCB)
&& (pState->pConnectPCB->snd_queuelen < TCP_SND_QUEUELEN))
{
//MEM_STATS_DISPLAY();
//TCP_STATS_DISPLAY();

// Here, we have data, and we have space. Set the total amount
// of data we will process to the lesser of data available or
// space available.
pState->pConnectPCB->flags |= (TF_NODELAY |TF_ACK_NOW);
Count = len;
if (tcp_sndbuf(pState->pConnectPCB) < Count)
{
Count = tcp_sndbuf(pState->pConnectPCB);
ASSERT(0);
}

// While we have data remaining to process, continue in this
// loop.
while ((Count)
&& (pState->pConnectPCB->snd_queuelen < TCP_SND_QUEUELEN))
{
//LEDOn(0); //d1

if (Count < TCP_MSS)
{
// Write the local buffer into the TCP buffer.
tcpErr = tcp_write(
pState->pConnectPCB, Data + Index, Count,
TCP_WRITE_FLAG_COPY /*| TCP_WRITE_FLAG_MORE*/); // 1 copy 2 more TCP_WRITE_FLAG_MORE
if(tcpErr != ERR_OK) {
ASSERT(0);
stam = Index+Count;
}
Index += Count;
Count = 0;
}
else
{
// Write the local buffer into the TCP buffer.
tcpErr = tcp_write(
pState->pConnectPCB, Data + Index,
TCP_MSS,
TCP_WRITE_FLAG_COPY | TCP_WRITE_FLAG_MORE); // 1 copy 2 more
if(tcpErr != ERR_OK) {
ASSERT(0);
stam = Index+Count;
}
Index += TCP_MSS;
Count -= TCP_MSS;
}
// Flush the data that has been written into the TCP output

tcpErr = tcpip_callback(tcp_output, pState->pConnectPCB);
pState->ui32LastTCPSendTime = 0; //g_SysTimeStamp;
if(tcpErr != ERR_OK) {
//ASSERT(0);
stam = Index+len;
}

}
//LEDOff(0); //d1

len -= Index;

  • Hi Shachar,
    Unfortunately, there is no plan to port any later LwIP versions to Tiva family. If the leak is caused by the LwIP then I will suggest you contact LwIP forum support for suggestions on how to handle them in LwIP 1.4.1. Have you tried to increase the heap and stack size and did you see any differences?