This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1114: OTP memory of the Flash Banks 0 and 7

Part Number: TMS570LS1114

Hello,

I have questions about the OTP. The TMS570LS1114 has two customers OTP memories. We want to use the OTP memories for our data. I read, that the first 16 byte of the OTP of Flash bank 0 contains a AJSM secure key. I assume that these bytes are not available for our data.

1) Is there any other double usage of the cutsomer OTP memory?

2) Can we use the OTP ranges 0xF000_0010 - 0xF000_0FFF and 0xF000_E000 - 0xF000_E7FF without further restrictions?

3) Is there an overwrite possible? Can a second write access clear further bits of the OTP memory?

Thanks,

Bernhard