Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
Hi there,
I'm compiling the following code on the TM4C123G LaunchPad via CCS 8.2.0.0007
#include <stdint.h>
#include <stdbool.h>
#define ROWS 2 //Number of rows
#define COLS 3 //Number of columns
#define PIXELS ROWS*COLS // Pixels in the strip
struct Node { //Build a structure for pointer, R, G, B
struct Node *Next;
uint8_t var1;
uint8_t var2;
uint8_t var3;
};
typedef struct Node NodeArr;
NodeArr theArray[ROWS][COLS];
NodeArr *HeadPt = &theArray[0][0];
NodeArr *pt;
pt = HeadPt;
while (1) {
}
}
Just at build, I get the following error messages:
CORTEX_M4_0: Trouble Reading Memory Block at 0x702001e7 on Page 0 of Length 0x4: Debug Port error occurred.
CORTEX_M4_0: Trouble Reading Memory Block at 0x702001e7 on Page 0 of Length 0x4: Debug Port error occurred.
CORTEX_M4_0: Trouble Reading Memory Block at 0x702001e7 on Page 0 of Length 0x4: Debug Port error occurred.
Two things:
- The memory space shown here is "external SRAM"!
- The same program compiles without issues on an online C-compiler (and runs) with no issues.
Any ideas why this might be happening?
Thanks for your attention!
DV