This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/EK-TM4C123GXL: I2C3 configuration

Part Number: EK-TM4C123GXL


Tool/software: Code Composer Studio

Hello, 

I am working on a project that consists on configuring a touch panel through i2C. I have to use the pins PD0 (SCL) and PD1 (SDA) of the connector J3 of the tiva. 

The communication seems not to work properly, so I would like to clarify the configuration I have made to be sure the issue is no comming from this.

I am working with RTOS. My init configuration of the i2C is the following :

 /* initiate touch i2c device */
    I2C_Params_init(&i2cparams);
    i2cparams.bitRate = I2C_100kHz;
    handle = I2C_open(EK_TM4C123GXL_I2C3,&i2cparams);
    if (handle == NULL) 
    {
        System_printf("I2C was not opened");
    }

Where the define EK_TM4C123GXL_I2C3 is refering to the following type from EK-TM4C123GXL.h :

/*!
* @def EK_TM4C123GXL_I2CName
* @brief Enum of I2C names on the EK_TM4C123GXL dev board
*/
typedef enum EK_TM4C123GXL_I2CName {
EK_TM4C123GXL_I2C0 = 0,
EK_TM4C123GXL_I2C3,

EK_TM4C123GXL_I2CCOUNT
} EK_TM4C123GXL_I2CName;

1) I am not sure I properly understand here if the I2C3 mentionned is really the one I would like to configure, could you confirm this ? 

I am calling the function Board_initI2C() in the main. I don't understand neither the code of this function (Board_initI2C, file EK-TM4C123GXL.c) : 

/*
 *  ======== EK_TM4C123GXL_initI2C ========
 */
void EK_TM4C123GXL_initI2C(void)
{
    /* I2C1 Init */
    /* Enable the peripheral */
    SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C1);

    /* Configure the appropriate pins to be I2C instead of GPIO. */
    GPIOPinConfigure(GPIO_PA6_I2C1SCL);
    GPIOPinConfigure(GPIO_PA7_I2C1SDA);
    GPIOPinTypeI2CSCL(GPIO_PORTA_BASE, GPIO_PIN_6);
    GPIOPinTypeI2C(GPIO_PORTA_BASE, GPIO_PIN_7);

    /* I2C3 Init */
    /*
     * NOTE: TI-RTOS examples configure pins PD0 & PD1 for SSI3 or I2C3.  Thus,
     * a conflict occurs when the I2C & SPI drivers are used simultaneously in
     * an application.  Modify the pin mux settings in this file and resolve the
     * conflict before running your the application.
     */
    /* Enable the peripheral */
    SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C3);

    /* Configure the appropriate pins to be I2C instead of GPIO. */
    GPIOPinConfigure(GPIO_PD0_I2C3SCL);
    GPIOPinConfigure(GPIO_PD1_I2C3SDA);
    GPIOPinTypeI2CSCL(GPIO_PORTD_BASE, GPIO_PIN_0);
    GPIOPinTypeI2C(GPIO_PORTD_BASE, GPIO_PIN_1);

    /*
     * These GPIOs are connected to PD0 and PD1 and need to be brought into a
     * GPIO input state so they don't interfere with I2C communications.
     */
    GPIOPinTypeGPIOInput(GPIO_PORTB_BASE, GPIO_PIN_6);
    GPIOPinTypeGPIOInput(GPIO_PORTB_BASE, GPIO_PIN_7);

    I2C_init();
}

This code seems to configure i2C3 with the pins PD0 and PD1.

2) Do I have to disable the configuration written in the same file for the SSI3 ?

I have noticed otherwise that on the Tiva board, there is two PD0 and PD1 pins. 

3) How do you know that you configure one or the others ? 

Thank you in advance for your help !

Best regards,

Elisabeth Tixier