Part Number: TMS570LS3137
I am attempting to test an ISR I have created to react to a positive edge triggered pulse on pin GIO A 1. Upon first attempt I succsfully observered my ISR execute as expected. However, upon subsequent tests, I was no longer able to flash software updates to the board. Some of the status lights remain lit when the Hercules Dev board is powered, so I'm assuming we did not smoke the board. Our procedure was to apply a 3.3V 1Hz squarewave signal to the pin which according to the processor specs is within the 3.2 to 3.6V range.
Is there any advice on injecting signals to the TMS570LS31x Hercules dev. board? I would like to get the current board repaired if possible; however, in the meantime I have order 5-additioal boards. I am reluctant, however, to perform the same test again without understanding how the failure occured. Any help would be greatly appreciated.
-robert