Hi,
Hope you are having good time.
I am working on boot_serial code configured via CAN for application upgrade.
As per the document "SW-TM4C-BOOTLDR-UG-2.1.4.178.pdf ", on Page No 5 it states
"When configured to use UART0, Ethernet, or USB, the LM Flash Programmer GUI can be used
to download an application via the boot loader."
I want to follow a similar approach via any tool for CAN. Can you please provide some inputs.
Best Regards,
Ramesh