Part Number: RM48L940
Other Parts Discussed in Thread: RM48L952
Hello,
i try to put FreeRTOS into operation on a RM48L952 and have the very same issue as user193949!
It seems that the debug probe interferes with execution time and leads to the following behaviour:
When I call vTaskDelay(1/portTICK_PERIOD_MS) to blink an LED, it blinks at a period of more than 100ms instead of 1ms.
When I use another value for vTaskDelay (e. g. 10/portTICK_PERIOD_MS for 10ms) the LED stays forever.
So I have seen that the issue was identified but is there a possibility to use the debug probe without having such unwanted behaviour?
Thanks for help
BR