Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN,
Hi,
I have a problem with the startup code in HL_sys_startup.c generated by HalCoGen.
The program runs into the while(1) loop inside esmGroup3Notification although there is actually no group 3 error.
The problem can be reproduced as follows:
- Create a new HalCoGen project for TMS570LC4357 without FreeRTOS and generated the code
- Create a new CSS project with the HalCoGen sources
- Set the optimization from “Off” to “0” (register optimization)
- Add an additional access to esm group 3 status register in user code (22) (see attachment)
- Load this project to HDK, then the program runs into the esmGroup3Notification
While debugging, I found that the register address of esm group 3 register (esmREG->SR1[2]) gets loaded to R4 when the code enters the switch case.
The assembler function _memInit_ uses this register without restoring its content. However, when the code tests the content of esm group 3 register afterwards, R4 points to a different memory location and an error is assumed although there is no group 3 error.
According to the ARM procedure call standard, “A subroutine must preserve the contents of the registers r4-r8, r10, r11 and SP” . This is not true for the _memInit_ function.
As a workaround, I changed the _memInit_ such that it uses the argument registers R1-R3 which do not need to be preserved.
Is there a plan to make _memInit_ compliant to procedure call standard?
Best regards,
Katharina Gilles
/** @file HL_sys_startup.c
* @brief Startup Source File
* @date 07-July-2017
* @version 04.07.00
*
* This file contains:
* - Include Files
* - Type Definitions
* - External Functions
* - VIM RAM Setup
* - Startup Routine
* .
* which are relevant for the Startup.
*/
/*
* Copyright (C) 2009-2016 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "HL_sys_common.h"
#include "HL_system.h"
#include "HL_sys_vim.h"
#include "HL_sys_core.h"
#include "HL_esm.h"
#include "HL_sys_mpu.h"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/* USER CODE BEGIN (2) */
/* USER CODE END */
/* External Functions */
/*SAFETYMCUSW 218 S MR:20.2 <APPROVED> "Functions from library" */
extern void __TI_auto_init(void);
/*SAFETYMCUSW 354 S MR:NA <APPROVED> " Startup code(main should be declared by the user)" */
extern int main(void);
/*SAFETYMCUSW 122 S MR:20.11 <APPROVED> "Startup code(exit and abort need to be present)" */
/*SAFETYMCUSW 354 S MR:NA <APPROVED> " Startup code(Extern declaration present in the library)" */
extern void exit(int _status);
/* USER CODE BEGIN (3) */
/* USER CODE END */
/* Startup Routine */
void _c_int00(void);
/* USER CODE BEGIN (4) */
/* USER CODE END */
#pragma CODE_STATE(_c_int00, 32)
#pragma INTERRUPT(_c_int00, RESET)
#pragma WEAK(_c_int00)
/* SourceId : STARTUP_SourceId_001 */
/* DesignId : STARTUP_DesignId_001 */
/* Requirements : HL_CONQ_STARTUP_SR1 */
void _c_int00(void)
{
/* USER CODE BEGIN (5) */
/* USER CODE END */
/* Initialize Core Registers to avoid CCM Error */
_coreInitRegisters_();
/* Initialize Stack Pointers */
_coreInitStackPointer_();
/* Reset handler: the following instructions read from the system exception status register
* to identify the cause of the CPU reset.
*/
switch(getResetSource())
{
case POWERON_RESET:
case DEBUG_RESET:
case EXT_RESET:
/* USER CODE BEGIN (6) */
/* USER CODE END */
/* Initialize L2RAM to avoid ECC errors right after power on */
_memInit_();
/* USER CODE BEGIN (7) */
/* USER CODE END */
/* USER CODE BEGIN (8) */
/* USER CODE END */
/* USER CODE BEGIN (9) */
/* USER CODE END */
/* Enable CPU Event Export */
/* This allows the CPU to signal any single-bit or double-bit errors detected
* by its ECC logic for accesses to program flash or data RAM.
*/
_coreEnableEventBusExport_();
/* USER CODE BEGIN (10) */
/* USER CODE END */
/* Check if there were ESM group3 errors during power-up.
* These could occur during eFuse auto-load or during reads from flash OTP
* during power-up. Device operation is not reliable and not recommended
* in this case. */
if ((esmREG->SR1[2]) != 0U)
{
esmGroup3Notification(esmREG,esmREG->SR1[2]);
}
/* Initialize System - Clock, Flash settings with Efuse self check */
systemInit();
/* USER CODE BEGIN (11) */
/* USER CODE END */
/* Enable IRQ offset via Vic controller */
_coreEnableIrqVicOffset_();
/* Initialize VIM table */
vimInit();
/* USER CODE BEGIN (12) */
/* USER CODE END */
/* Configure system response to error conditions signaled to the ESM group1 */
/* This function can be configured from the ESM tab of HALCoGen */
esmInit();
/* USER CODE BEGIN (13) */
/* USER CODE END */
break;
case OSC_FAILURE_RESET:
/* USER CODE BEGIN (14) */
/* USER CODE END */
break;
case WATCHDOG_RESET:
case WATCHDOG2_RESET:
/* USER CODE BEGIN (15) */
/* USER CODE END */
break;
case CPU0_RESET:
/* USER CODE BEGIN (16) */
/* USER CODE END */
/* USER CODE BEGIN (17) */
/* USER CODE END */
/* USER CODE BEGIN (18) */
/* USER CODE END */
/* Enable CPU Event Export */
/* This allows the CPU to signal any single-bit or double-bit errors detected
* by its ECC logic for accesses to program flash or data RAM.
*/
_coreEnableEventBusExport_();
/* USER CODE BEGIN (19) */
/* USER CODE END */
break;
case SW_RESET:
/* USER CODE BEGIN (20) */
/* USER CODE END */
break;
default:
/* USER CODE BEGIN (21) */
/* USER CODE END */
break;
}
/* USER CODE BEGIN (22) */
if ((esmREG->SR1[0]) != 0U)
{
esmGroup1Notification(esmREG,esmREG->SR1[0]);
}
if ((esmREG->SR1[1]) != 0U)
{
esmGroup2Notification(esmREG,esmREG->SR1[1]);
}
if ((esmREG->SR1[2]) != 0U)
{
esmGroup3Notification(esmREG,esmREG->SR1[2]);
}
/* USER CODE END */
_mpuInit_();
/* USER CODE BEGIN (23) */
/* USER CODE END */
_cacheEnable_();
/* USER CODE BEGIN (24) */
/* USER CODE END */
/* USER CODE BEGIN (25) */
/* USER CODE END */
/* initialize global variable and constructors */
__TI_auto_init();
/* USER CODE BEGIN (26) */
/* USER CODE END */
/* call the application */
/*SAFETYMCUSW 296 S MR:8.6 <APPROVED> "Startup code(library functions at block scope)" */
/*SAFETYMCUSW 326 S MR:8.2 <APPROVED> "Startup code(Declaration for main in library)" */
/*SAFETYMCUSW 60 D MR:8.8 <APPROVED> "Startup code(Declaration for main in library;Only doing an extern for the same)" */
main();
/* USER CODE BEGIN (27) */
/* USER CODE END */
/*SAFETYMCUSW 122 S MR:20.11 <APPROVED> "Startup code(exit and abort need to be present)" */
exit(0);
/* USER CODE BEGIN (28) */
/* USER CODE END */
}
/* USER CODE BEGIN (29) */
/* USER CODE END */
/* USER CODE BEGIN (30) */
/* USER CODE END */