Other Parts Discussed in Thread: HALCOGEN
Using TMS570LS3137ZWT HDK with on-board SDRAM.
I have used halcogen+CCS to generate a project trying to access the EMIF SDRAM via address 0x80000000. I have tried with the jumper cables connected as well as disconnected (the schematic shows the jumper provides power to the SDRAM).
EMIF Driver is enabled under the Driver Enable tab.
EMIF is enabled under the PINMUX tab.
I have Enabled EMIF SDRAM under the EMIF General tab.
The EMIF SDRAM tab i left at the defaults (may be part of the problem?).
I have been attempting to write and read from the address 0x80000000+. While using a logic analyzer on the EMIF pins, they are outputting signals so i know it is trying.
Any help would be appreciated.
Thanks,
David Cothran