Part Number: EK-TM4C1294XL
Tool/software: Code Composer Studio
Hi,
I'm trying to calibrate my screen, the buttons are responding in the wrong locations (a bit off on the left side). But I can't find any application to do that.
This link mentions a "calibrate application", but I couldn't find any (and the link inside the PDF to explain the calibration is broken).
There's at least something that helps with the calibration? Because the touch.c has many numbers and do not explain what they actually do (I imagined it would be just X, Y and Z, three numbers).
#ifdef LANDSCAPE
328192, // M0
-4352, // M1
-178717056, // M2
1488, // M3
-314592, // M4
1012670064, // M5
3055164, // M6
#endif
Regards,
Helder