Part Number: EK-TM4C123GXL
Hello,
My I2C interface is not firing up at all. The compiler just runs the main code and stops. Following is my code,
#include <stdarg.h>
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_i2c.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "driverlib/i2c.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
//*********************************************************** Global ************************************************************************//
int i;
uint8_t Fifo_WR_PTR;
uint8_t Fifo_RD_PTR;
uint16_t Num_Samples_Available;
uint16_t Num_Samples_Read;
uint8_t ir1;
uint8_t ir2;
uint8_t red1;
uint8_t red2;
uint16_t ir;
uint16_t red;
//************************************************** Initialize I2C module 0 ***************************************************************//
void InitI2C0(void)
{
//enable I2C module 0
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C0);
//reset module
SysCtlPeripheralReset(SYSCTL_PERIPH_I2C0);
//enable GPIO peripheral that contains I2C 0
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
// Configure the pin muxing for I2C0 functions on port B2 and B3.
GPIOPinConfigure(GPIO_PB2_I2C0SCL);
GPIOPinConfigure(GPIO_PB3_I2C0SDA);
// Select the I2C function for these pins.
GPIOPinTypeI2CSCL(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_3);
// Enable and initialize the I2C0 master module. Use the system clock for
// the I2C0 module. The last parameter sets the I2C data transfer rate.
// If false the data rate is set to 100kbps and if true the data rate will
// be set to 400kbps.
I2CMasterInitExpClk(I2C0_BASE, SysCtlClockGet(), true);
//clear I2C FIFOs
HWREG(I2C0_BASE + I2C_O_FIFOCTL) = 80008000;
}
//************************************************** I2C Send function ***************************************************************//
void I2CSend(uint16_t device_address, uint16_t device_register, uint8_t device_data)
{
//specify that we want to communicate to device address with an intended write to bus
I2CMasterSlaveAddrSet(I2C0_BASE, device_address, false);
//register to be read
I2CMasterDataPut(I2C0_BASE, device_register);
//send control byte and register address byte to slave device
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
//wait for MCU to finish transaction
while(I2CMasterBusy(I2C0_BASE));
I2CMasterSlaveAddrSet(I2C0_BASE, device_address, false);
//specify data to be written to the above mentioned device_register
I2CMasterDataPut(I2C0_BASE, device_data);
//wait while checking for MCU to complete the transaction
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
//wait for MCU & device to complete transaction
while(I2CMasterBusy(I2C0_BASE));
}
//************************************************** I2C Single Receive function ***************************************************************//
uint32_t I2CReceiveS(uint32_t slave_addr, uint8_t reg)
{
//specify that we are writing (a register address) to the slave device
I2CMasterSlaveAddrSet(I2C0_BASE, slave_addr, false);
//specify register to be read
I2CMasterDataPut(I2C0_BASE, reg);
//send control byte and register address byte to slave device
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
//wait for MCU to finish transaction
while(I2CMasterBusy(I2C0_BASE));
//specify that we are going to read from slave device
I2CMasterSlaveAddrSet(I2C0_BASE, slave_addr, true);
//send control byte and read from the register we specified
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
//wait for MCU to finish transaction
while(I2CMasterBusy(I2C0_BASE));
//return data pulled from the specified register
return I2CMasterDataGet(I2C0_BASE);
}
//************************************************** I2C Burst Receive function ***************************************************************//
uint32_t I2CReceiveB(uint32_t slave_addr, uint8_t reg)
{
//specify that we are writing (a register address) to the slave device
I2CMasterSlaveAddrSet(I2C0_BASE, slave_addr, false);
//specify register to be read
I2CMasterDataPut(I2C0_BASE, reg);
//send control byte and register address byte to slave device
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
//wait for MCU to finish transaction
while(I2CMasterBusy(I2C0_BASE));
//specify that we are going to read from slave device
I2CMasterSlaveAddrSet(I2C0_BASE, slave_addr, true);
//send control byte and read from the register we specified
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
//wait for MCU to finish transaction
while(I2CMasterBusy(I2C0_BASE));
//return data pulled from the specified register
return I2CMasterDataGet(I2C0_BASE);
}
//************************************************** Slave Fifo Reset Function ***************************************************************//
void resetFifo ()
{
I2CSend(0x57, 0x02, 0x00); // Reset FIFO Write Pointer
I2CSend(0x57, 0x04, 0x00); // Reset FIFO Read Pointer
I2CSend(0x57, 0x03, 0x00); // Reset FIFO Overflow Counter
}
//************************************************** I2C Interrupt Handler Function ***************************************************************//
void I2C0MasterIntHandler (void)
{
I2CMasterIntClear(I2C0_BASE); // Clear the I2C interrupt flag
resetFifo(); // Reset Slave Fifo
Fifo_WR_PTR = I2CReceiveS(0x57, 0x02); // Read FIFO Write Pointer
Num_Samples_Available = Fifo_WR_PTR - Fifo_RD_PTR; // Evaluating Number of samples to be read from FIFO
// Num_Samples_Read =< Num_Samples_Available; //
for (i = 0; i < Num_Samples_Available; i++)
{
ir1 = I2CReceiveB(0x57, 0x05); // Receive first byte of sample
ir2 = I2CReceiveB(0x57, 0x05); // Receive second byte of sample
ir = (uint16_t) ir1 << 16 | (uint16_t) ir2; // Complete iR sample
red1 = I2CReceiveB(0x57, 0x05); // Receive third byte of sample
red2 = I2CReceiveB(0x57, 0x05); // Receive fourth byte of sample
red = (uint16_t) red1 << 16 | (uint16_t) red2; // Complete Red sample
}
}
//************************************************************* Main **************************************************************************//
int main()
{
SysCtlClockSet(SYSCTL_SYSDIV_10 | SYSCTL_USE_PLL | SYSCTL_OSC_INT | SYSCTL_XTAL_16MHZ); // System Clock
InitI2C0(); // I2C Initialization
resetFifo(); // Reset Slave Fifo
I2CSend(0x57, 0x06, 0x03); // Mode Configuration
I2CSend(0x57, 0x07, 0x47); // SpO2 Configuration
I2CSend(0x57, 0x09, 0x44); // LEDs Configuration
I2CSend(0x57, 0x00, 0xB1); // Interrupt Status
I2CSend(0x57, 0x01, 0xB0); // Interrupt Enable
}
I have no clue what is wrong. Any help would be appreciated. Thank you for your time!!