Other Parts Discussed in Thread: TMS570LS3137,
Hello,
We're using several TMS570LS/LC devices and need to understand the following due to our software team has a concern the difference in ARM cores shall cause software maintenance issues.
Questions -
1. Is there a whitepaper which describes if the Software can be backward or upward compatible between the LS and LC series ?
2. Is the a QFP version of LC series on the way or sampling ?
-- In project 2 we cannot use the BGA version as we are using thick copper layers and we cannot have such fine pitch BGA .
Project 1: We're using TMS570LS3137 in QFP Package - ARM Core R4F, 160MHz max
Project 2: : Now-Using TMS570LS3137 in BGA Package ARM Core R4F, 180 MHz max - But would like to upgrade to TMS570LC4357 , BGA Package , ARM Core R5F, 300 MHz Max.