Part Number: TM4C129ENCPDT
Tool/software: TI C/C++ Compiler
Hi,
I've built a project based upon the enet_weather example program which is working. I've added support for SMTP and some UDP commands along with some other application code. I'm trying to add TELNET capability to the project. I found some TELNET code in location c:ti/TivaWare_C_Series-2.1.4.178/third_party/uip-1.0/apps/telnetd directory. I added a path to the telnetd directory in the ARM Compiler - Include Options. The telnetd directory contains the files telnetd.c, telnetd.h, shell.c, and shell.h. I also added entries to the ARM Compile - Include Options to all access to a couple of other include files listed in the telnet and shell files. I'm able to compile the program successfully but it consistently fails when I add the function telnetd_init() to my code while linking. In my Console Window I see it's Invoking: ARM Linker. I'm getting error 10234-D : unresolved symbol remains and error 10010 : errors encountered during linking. It's failing because telnetd_init() is appearing as an unresolved symbol.
I assume I need to add some entry to the ARM Linker - File Search Path, either to --library or to --search path but I don't know what to add to either of these two windows in order to resolve the issue of my object file referencing telnetd_init because it's unable to find the definition for the function.
As a reference I'm using snmp_init() successfully in my project which is in location c:ti/TivaWare_C_Series-2.1.4.178/third_party/lwip-1.4.1/src/core/snmp directory in the file msg_in.c. I'm able to compile and link this file and that function into my project with what appears to me to be the default setting in the ARM Linker - File Search Path windows. In my ARM Linker I have a path to driverlib.lib, libc.a and also to CG_TOOL_ROOT/ lib and /include.
I would prefer to reference these files from the Telnetd directory than to make a copy and add them into my project which I would hope would actually work.
Any suggestions on how to get the TELNETD files to Link into my project would be greatly appreciated. I've searched up and down the forum for a possible solution without any luck