Part Number: SIMPLELINK-SDK-VOICE-DETECTION-PLUGIN
Tool/software: Code Composer Studio
Hello,
I'm evaluating the SimpleLink SDK Voice detection plugin with the MSP432 microcontroller with Sharp display as described in the SDK user manual. I was able to run the nortos examples successfully, and I have tested the voice command detection VCD feature of the SDK extensible.
Part of my evaluation is also to recommend a VAD library that will be used in our new proof of concept device. The documentation of the SDK mentions that it has a stand-alone VAD module and is part of the example provided to demonstrate the VCD feature.
Unfortunately, the VAD specific API calls are not explicitly demonstrated. I was wondering it is there's a sample application and/or more information on how to use the standalone VAD library. In my opinion, the API document covering the VAD section is not sufficient to be able to understand and reliably use the VAD in standalone mode.
Is the VAD portable to the TM4C129x series microcontroller since this processor is at the center of our current hardware platform for our new proof of concept?
Any information would be appreciated,
Thanks,
David N.