Part Number: TM4C123GE6PM
Hi, This is Namha.
I have an issue implementing the multi-channel ADC interrupt function.
I would like to use two ADC interrupt handlers using timer0 and 1.
(ADC sampling frequency :1Mhz)
But ADC0SS3IntHandler only works and ADC1SS3IntHandler does not work.
ADC initialization and handler code are attached below. Is it a setting problem or another problem?
//--------------------------------------- ADC initialization -----------------------------------------------//
void ADCInit(void)
{
//Initialize ADC
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0); //ADC peripheral
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1); //ADC peripheral
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1);
//Pins used for ADC channels
ROM_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0);
// *** ADC
ROM_ADCReferenceSet(ADC0_BASE,ADC_REF_INT);
ROM_ADCReferenceSet(ADC1_BASE,ADC_REF_INT);
ROM_ADCSequenceConfigure(ADC0_BASE,3,ADC_TRIGGER_TIMER,0);
ROM_ADCSequenceConfigure(ADC1_BASE,3,ADC_TRIGGER_TIMER,3);
ROM_ADCSequenceStepConfigure(ADC0_BASE, ADC_SEQUENCE_NUMBER, 0, ADC_CTL_D | ADC_CTL_CH0 | ADC_CTL_IE | ADC_CTL_END);
ROM_ADCSequenceStepConfigure(ADC1_BASE, ADC_SEQUENCE_NUMBER, 0, ADC_CTL_D | ADC_CTL_CH1 | ADC_CTL_IE | ADC_CTL_END);
ROM_ADCSequenceEnable(ADC0_BASE, ADC_SEQUENCE_NUMBER);
ROM_ADCSequenceEnable(ADC1_BASE, ADC_SEQUENCE_NUMBER);
//ROM_ADCHardwareOversampleConfigure(ADC0_BASE, txLeakageOversamplingNumber);
//ROM_ADCHardwareOversampleConfigure(ADC1_BASE, txLeakageOversamplingNumber);
// *** Timer0
ROM_TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
samplePeriod = ROM_SysCtlClockGet()/(1000*ADC_MAX_SAMPLING_RATE);
ROM_TimerLoadSet(TIMER0_BASE, TIMER_A, samplePeriod - 1); // sampling frequency 1Mhz
ROM_TimerControlTrigger(TIMER0_BASE, TIMER_A, true);
// *** Timer1
ROM_TimerConfigure(TIMER1_BASE, TIMER_CFG_PERIODIC);
ROM_TimerLoadSet(TIMER1_BASE, TIMER_A, samplePeriod - 1); // sampling frequency 1Mhz
ROM_TimerControlTrigger(TIMER1_BASE, TIMER_A, true);
// *** Interrupts
ROM_IntEnable(INT_TIMER0A);
ROM_IntEnable(INT_TIMER1A);
ROM_TimerIntEnable(TIMER0_BASE,TIMER_TIMA_TIMEOUT);
ROM_TimerIntEnable(TIMER1_BASE,TIMER_TIMA_TIMEOUT);
ROM_IntEnable(INT_ADC0SS3);
ROM_IntEnable(INT_ADC1SS3);
ROM_ADCIntEnable(ADC0_BASE,ADC_SEQUENCE_NUMBER);
ROM_ADCIntEnable(ADC1_BASE,ADC_SEQUENCE_NUMBER);
ROM_IntMasterEnable();
ROM_TimerEnable(TIMER0_BASE,TIMER_A);
ROM_TimerEnable(TIMER1_BASE,TIMER_A);
}
//--------------------------------------------------------- Handler -------------------------------------------------------------------//
void Timer0IntHandler(void)
{
ROM_TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
}
void Timer1IntHandler(void)
{
ROM_TimerIntClear(TIMER1_BASE, TIMER_TIMA_TIMEOUT);
}
void ADC0SS3IntHandler(void)
{
ROM_ADCIntClear(ADC0_BASE,3);
ADC0Value[0] = 0;
ROM_ADCSequenceDataGet(ADC0_BASE,3,ADC0Value); // Get Data from ADC and store it in ADC1Value
adcRawData_0[ADCCurrentIndex_0] = *ADC0Value;
ADCCurrentIndex_0++;
if(ADCCurrentIndex_0 >= 2048)
{
ADCCurrentIndex_0 = 0;
}
}
void ADC1SS3IntHandler(void)
{
ROM_ADCIntClear(ADC1_BASE,3);
ADC1Value[0] = 0;
ROM_ADCSequenceDataGet(ADC1_BASE,3,ADC1Value); // Get Data from ADC and store it in ADC1Value
adcRawData_1[ADCCurrentIndex_1] = *ADC1Value;
ADCCurrentIndex_1++;
if(ADCCurrentIndex_1 >= 2048)
{
ADCCurrentIndex_1 = 0;
}
}
Thank you.