Part Number: TMS570LC4357
I have question(s) about the TMS570LC4357 and its use of JTAG, via the XDS200:
[Q1] What is the minimum required JTAG Signals for debugging and programming the MCU?
[Q2] Can we get away without using the RTCK JTAG signal? If so, how do we handle that RTCK on the MCU side and XDS200 side? Or is RTCK 100% required?
[Q3] In the buffered JTAG signal case, will a simple OR-gate ic work (like a 74LVC1G32)?
[Q4] Using the buffered JTAG signals, what is the max length (in) between the Target MCU (TMS570…) and the XDS200 20-pin connector we can have.
[Q5] If power is not present on the Target, can the XDS200 provide power to the target MCU to allow JTAG programming of the flash program memory?
Thanks,
R. Wright