Part Number: TMS570LC4357
Hello,
I would like to execute STC1 with multiple segments :
- 125 intervals STC1 Segment 0 (CPU)
- 3 intervals of STC1 Segment1 (uSCU).
Is it possible to execute sequentially the 2 segments or each segment must be tested individually?
If 2 segments can be tested sequentially :
Which register must be configured in this case : INTCOUNT of STCGCR0 register with value 0x80 (125 + 3)?
If each segment is tested individually,
Which register is configured in this case to select the segment to test? SEGID_PLOAD bits in STCSEGPLR register?
Best regards,
François