Part Number: TMS570LC4357
Hello,
I have some questions about CPU reset during LBIST
In TMS570 Technical Reference Manual (chapter 10.9.1 Example: STC1 Self-Test Run)
--> If BOTH Cores are configured in parrallel during the STC1 Segment0 seltest (SEG0_CORE_SEL = 0x0), there's only 1 or 2 CPU reset at the end of the selftest?
--> in case of CPU reset what's happen : all TMS is reseted or only internal ARM core?
--> If only ARM core is reseted, Software in FPROM starts in address 0x0 after the CPU(s) reset?
In chapter 10.10 (Self-Test Controller Diagnostics)
--> For steps2 or 3 or 4 or 5 is there a CPU reset after the completion of each Selftest?