Part Number: TMS570LC4357
Hello,
In Datasheet, it is mentionned there are two slave ports (Flash_PortA and Flash_PortB) to access to the flash memory.
To read in FPROM Bank0 and 1:
1- Which port is configured by default? Port A, PortB or Both? if BOTH, how is it managed?
2- Is it necessary that Software configure the port Access? Which TMS registers must be used to configure it?
Best regards,
François