Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Tool/software: TI-RTOS
Hello,
I have been into this problem for two weeks. Please I need help.
I want to run an encryption algorithm on TMS570LC. I generated code by Halcogen, I use CCS8.3 and XDC Tools.
The program is as follow:
#include "api.h"
#include <stdio.h>
#include <stdint.h>
#include <string.h>
#define MLEN 59
static unsigned long long overflowcnt = 0;
int main(void)
{
unsigned char sk[CRYPTO_SECRETKEYBYTES];//CRYPTO_SECRETKEYBYTES = 2500
unsigned char pk[CRYPTO_PUBLICKEYBYTES]; // CRYPTO_PUBLICKEYBYTES =4500
unsigned char sm[MLEN+CRYPTO_BYTES];
unsigned long long smlen;
unsigned int t0, t1;
// Key-pair generation
crypto_sign_keypair(pk, sk);
The problem is that the program shows no results. When I suspend the execution I found the prog stack here in B DataEntry in the file HL_Sysintvec.asm which is generated by HalcoGen.
;-------------------------------------------------------------------------------
; interrupt vectors
resetEntry
b _c_int00
undefEntry
b undefEntry
svcEntry
b svcEntry
prefetchEntry
b prefetchEntry
dataEntry
b dataEntry
b phantomInterrupt
ldr pc,[pc,#-0x1b0]
ldr pc,[pc,#-0x1b0]
;-------------------------------------------------------------------------------
I increased the Heap to 20000. But the problem persists. Also the memory allocation shows :
My program is a very ordinary program that is executed on computer before. That means it does need to access any special memory location on the chip. I just want to take the measurement of performance on the chip.
I am beginner in this domain. Please, I need your help
How can I solve this problem.
Bes,
Soundes.