This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DK-TM4C129X: Can we build PAN profile or NAP based on DK-TM4C129X and CC2564 module

Part Number: DK-TM4C129X

Hi,

I have DK-TM4C129X and CC2564 module. And want to implement PANU based on bluetopia stack. The Bluetooth PAN/BNEP allows to send/receive Ethernet frames. To be useful, these packets need to be integrated with a network stack. There is one example of PANU demo using bluetopiaPM on linux platform.

Can i use the same panu network interface of bluetopia with lwip TCP/IP stack on DK-TM4C129X? And where will i find the source code for BluetopiaPM PANU demo?

Thanks and regards,

Bhagyashri