Part Number: TMDS570LS31HDK
Other Parts Discussed in Thread: HALCOGEN, TMS570LS3137
Tool/software: Code Composer Studio
I have configured SPI2 as a master and SPI4 as a slave with complementary attributes.
I have connected them externally but I do not even get output from SPI2. I see SPI2 is connected to an SD slot. Is this causing a problem?
I have used the NHET 100, 102 and 103 on J11 in place of the SPI4 inputs CLK, CS0 and SIMO respectively.
The SPI2 outputs are marked on the J10.