Part Number: TMS570LC4357
while I'm using the EMAC module to transmit and receive message,I have 3 steps:
1.send ARP package and receive to build the link between the PC and the board.
2.If step1 is OK,put the message into the buffer.
3,configure the registers of the EMAC module to transmit the message.
But if I run the code twice ,the EMACSTATUS register become 00500000.
Is it because I didn't receive the ARP package from the PC so that I didn't build up the link?