This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP-EXPCC430RFX: MSP-EXPCC430RF4

Part Number: MSP-EXPCC430RFX

Tool/software: Code Composer Studio

I set the register (sysctl) to 1 and download it to the board successfully. However, the ccs shows "MSP430: Error connecting to the target: Could not find device (or device not supported)" .

MSP430: Error connecting to the target: Could not find device (or device not supported)

The version of ccs is the latest and I had successfully download many times before the error occurrs. I think it is related to the SYSCTL  and the JATG!

  • after I download other files to the board, the ccs shows "MSP430: Error connecting to the target: Could not find device (or device not supported)"
  • Hello Li,

    How did you download the code to the board successfully? Was it working before you programmed it?

    It looks like there are switches on the board that control which MCU you are programming, either the base board or the satellite board. Have you double checked these switches so that you are programming the correct MCU? See Sections 2.1 of the MSP-EXPCC430RFX User's Guide. www.ti.com/.../slau460

    Thanks,
    JD
  • I had resolved this problem last night. The problem may be that the JTAG is occupied so that I can't download by JTAG or just because of some other mistakes in the program. Anyway, I hold the reset button and then used the msp430flasher to erase the flash, after many times trying it works. The flash was finally erased and the problem was solved.